AXIS#.PL.CMD

Description

AXIS#.PL.CMD reads the position command as it is received in the position loop entry.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units Rotary: counts, rad, deg, custom units, 16-bit counts. See Position Units for details.
Range Depends on units. See Position Range for details.
Default Value N/A
Data Type Float
See Also AXIS#.PL.FB
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.CMD

5900

170C

Signed32

Read Only

Position

AXIS2.PL.CMD

71436

1170

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.CMD

5900

Signed32

Read Only

Position

Related Topics

AXIS#.PL.ERR | AXIS#.PL.ERRFTHRESH | AXIS#.PL.ERRWTHRESH |

Position Loop